Back to case studies
UV-C Disinfection Robots Eliminate 99% of Surface Viruses in High-Traffic Facilities
Addressing facility hygiene with autonomous UV-C technology
High-traffic facilities such as retailers, gyms, and hospitality venues need consistent, verifiable cleaning processes to help protect staff and visitors. During the pandemic, many businesses relied heavily on manual sanitization, requiring employees to clean surfaces by hand across large, busy environments. This approach was time-consuming, difficult to validate, and created gaps in coverage during peak hours or overnight shifts.
To improve consistency and traceability, OMRON partnered with UV Systems UK to introduce autonomous UV-C Disinfection Robots for commercial facilities. Using precision UV-C lamps and advanced navigation, the robots can move through a space without manual operation, disinfecting exposed surfaces and logging completed areas for reporting.
In a 100,000 sq. ft. supermarket, a single robot can complete a disinfection cycle in approximately 2–3 hours while eliminating up to 99% of viruses and other pathogens on exposed surfaces. Unlike chemical-based cleaning processes, UV-C disinfection reduces the need for harsh substances and limits the amount of repetitive manual work required from staff.
The robots are designed for safe operation in active commercial environments. Integrated sensors detect obstacles and automatically stop the robot if a person enters the operating area. Wi-Fi connectivity also allows facility managers to access real-time reports, verify completed disinfection routes, and quickly identify any missed areas.
By automating part of the sanitization workflow, businesses can improve cleaning consistency, support regulatory requirements, and provide greater confidence for employees and customers. The solution also allows staff to focus on higher-value work rather than repetitive cleaning tasks. With a long service life and proven efficacy against pathogens including Covid, SARS, MERS, and Ebola, UV-C Disinfection Robots provide a traceable approach to hygiene for facilities with demanding cleaning needs.
Watch Topline’s story:
Download in: German | Spanish | French | Polish | Turkish
“With a minimum ten-year lifespan and the ability to eliminate all bacteria and viruses, the UV-C Robot is the only proven method to kill Covid on all surfaces and touchpoints of indoor work and leisure spaces. It is set to play a critical role in helping British businesses protect their customers, staff and brand for years to come.” — Andrew Hunt, CEO of UV Systems Ltd.
Results at a glance:
- Up to 99% reduction in surface virus contamination
- Ceiling-to-floor coverage in 2–3 hours for large facilities
- Traceability and reporting for completed disinfection areas
- Reduced manual cleaning bottlenecks and chemical exposure
- Safe, efficient overnight disinfection without added labor
Practical automation for facility hygiene
Maintaining hygiene in high-traffic facilities requires a balance of consistency, safety, and operational efficiency. OMRON’s autonomous disinfection solutions help businesses strengthen cleaning workflows with traceable UV-C technology that can be integrated into existing facility protocols.
If your team is exploring ways to improve disinfection consistency, reduce manual cleaning demands, or support safer facility operations, we can help identify an approach that fits your environment.