Back to news

OMRON Announces Significant Expansion and Upgrade to Collaborative Robot Lineup and Software 

News
12/4/2025
OMRON TM6S TM20S TM25S and TM30S Launch Banner

Elevating automation with next-generation robotics and smarter software

Pleasanton, California — December 12, 2025 — OMRON Robotics and Safety Technologies has announced a major expansion and upgrade to its TM S Series of collaborative robots. This comprehensive release introduces three new high-performance robots—the TM30S, TM20S, and TM6S—alongside critical hardware enhancements and the launch of the powerful TMflow 2.22 software platform.

These upgrades underscore our commitment to delivering flexible, safe, and intelligent automation solutions that directly address the growing demand for high-mix, low-volume production and critical labor shortages across global manufacturing sectors.

Next generation power and payload

The expansion of the OMRON TM S Series significantly broadens the range of demanding tasks that can be automated collaboratively:

Explore all OMRON TM S Series robots here—find the right cobot for your application.

  • OMRON TM30S Graphics with Features
  • OMRON TM6S cobot shown with built-in vision, 6 kg payload, 1,800 mm reach, IP65 arm (ISO Class 3), 35 kg arm weight, and 33 advanced safety functions.
  • OMRON TM20S heavy-duty automation cobot featuring built-in vision, 20 kg payload capacity, 1,300 mm reach, IP65/IP54 arm (ISO Class 3), 33 kg arm weight, and UL/CSA/ISO 13849-1 certified safety.

Hardware innovations for reliability and precision

The entire S Series line receives key hardware updates focused on making the robots more robust, precise, and adaptable for diverse industrial settings:

“With the launch of the TM6S, TM20S, TM25S, and TM30S—plus major hardware upgrades like IP65 protection across the entire Series, including the TM5S, TM7S, TM12S, and TM14S—and an integrated joint‑6 force torque sensor on the TM25S and TM30S, we’re enabling customers to tackle their toughest jobs with more safety, precision, and flexibility than ever.” — Qiqi Wang, Global Product Manager 

Intelligence upgraded: Introducing TMflow 2.22

The new TMflow 2.22 software update enhances the platform’s intuitive user experience while integrating powerful new functionalities:

Find out how TMflow 2.22 can elevate your automation—see all updates.

About OMRON Robotics and Safety Technologies

OMRON Robotics is a global leader and key division of OMRON Corporation, dedicated to pioneering the next generation of industrial automation through advanced robotics solutions. With over 40 years of expertise and more than 46,000 robots deployed worldwide, OMRON provides a comprehensive portfolio structured around the philosophy: “To the machine, the work of the machine. To man, the thrill of further creation.”

Our product lines include Autonomous Mobile Robots (AMRs) for dynamic material logistics, Collaborative Robots for safe human-robot teamwork, and high-speed Fixed Industrial Robots (SCARA, Delta, and Articulated arms) for precision assembly and sorting. OMRON Robotics empowers manufacturers to build flexible, high-quality, and agile production lines by delivering solutions engineered to coordinate seamlessly and meet evolving market demands.

Back to news

rss

Stay connected

form robot background