Back to case studies

Collaborative Palletizer Handles Up to 8 Boxes per Minute, Accelerating ROI for Industrial Manufacturers 

Case Study
1/8/2023
Collaborative palletizer boosting efficiency in manufacturing environment
reorder–reorder-arrow-move-arrange
Industry

Food & Commodities

update
Application

Palletizing

traffic
Robot Solution

OMRON TM12 & TM14 Cobot

Meeting the demand for safer, more flexible palletizing in dynamic production environments

A major European manufacturer faced persistent challenges with manual palletizing: operators were regularly exposed to heavy lifting, repetitive strain, and the need to frequently reconfigure lines for new products. Traditional palletizing systems required fixed installations and safety fencing, limiting adaptability and slowing changeovers.

To address these needs, FlexLink and OMRON partnered to engineer a collaborative palletizer with a compact footprint and active safety features. The system integrates OMRON cobots—either TM12 or TM14 models—capable of handling boxes up to 12kg and supporting both US and Euro pallet standards. Unlike conventional solutions, the collaborative palletizer is self-supporting and mobile, allowing it to be moved between production areas and installed in just one or two days.

With CE-certified safety controls, operators work safely alongside the robot—no fencing or laser scanners required. The dual-pick vacuum gripper boosts throughput to 14 parts per minute, with the standard setup achieving 8 boxes per minute. Automating palletizing reduces injury risk and allows staff to focus on higher-value tasks.

Since implementation, the manufacturer has seen a measurable increase in line productivity and a significant reduction in manual handling injuries. The investment has delivered a return in under two years, establishing the collaborative palletizer as a pivotal solution for agile, high-output manufacturing.

Watch FlexLink’s story:

Download in: Italian | German | Spanish | French | Polish | Turkish

“This solution meets the need for automated palletisation, which relieves the operators from this repetitive task so that they can focus on tasks with more added value, and that are more interesting.” — Gary Hinault, FlexLink’s Controls Engineer 

  • Collaborative palletizer automating box handling in industrial setting
  • Collaborative robot boosting efficiency in manufacturing environment
  • Operator Panel for Palletizing Solution
  • Collaborative palletizer installed on a flexible production line
  • Operator working safely alongside collaborative palletizer
  • Close-up of collaborative palletizer gripper handling cartons

Results at a glance:

Tailored automation for evolving production needs

FlexLink and OMRON continue to refine the collaborative palletizer, based on real-world feedback from manufacturers to ensure our solutions stay practical and effective. If you’re exploring ways to improve palletizing or want to create a safer, more flexible production line, we’d love to hear about your goals. Share your questions or project ideas with us anytime; our team is here to help you find the right solution for your facility.

Back to case studies

rss

Book a consultation

form robot background